Output Control
| Output Response Speed | Select the response speed of the internal amplifier according to the load conditions and how you will use the instrument. Slow – High-stability response. Select this to provide stable power to a variety of loads. Medium (default) – Normal speed response. Select this for applications covering a range of frequencies from commercial power line frequencies to the frequencies used by ship and aircraft power supplies. Fast – High-speed response. Select this for applications that require fast rise and fall speeds of power supplies. |
| Output Impedance | Enable (On) or disable (Off) the output impedance control. By programming an output impedance, you can
simulate the same environment as that provided by commercial power supplies. Resistance – Set the resistance parameter for all phases or each phase individually. Reactance – Set the reactance parameter for all phases or each phase individually. |